AXIS#.MOTOR.TEMPFAULT

Description

This parameter is used to configure the motor temperature fault level as a resistance threshold of the motor thermal sensor.

A zero value prevents temperature faults from being reported.

Context

For more information see Motor and Motor Temperature View.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Range

0 to 2,000,000,000 Ω

Default Value

2000

Data Type

Integer

See Also

AXIS#.MOTOR.TEMP
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
AXIS1.MOTOR.TEMPFAULT

500bh

1dh

Unsigned32

-

-

Read/Write

No

AXIS2.MOTOR.TEMPFAULT

510bh

1dh

Unsigned32

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.MOTOR.TEMPFAULT

6218

184A

Unsigned32

Read Only

-

AXIS2.MOTOR.TEMPFAULT

71754

1184

Unsigned32

Read Only

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.MOTOR.TEMPFAULT

6218

Unsigned32

Read Only

-